19.6.2 Steps for Porting an MCC Project

  1. Follow the steps outlined in the Porting Guide to migrate the application from WBZ351 to PIC32CX5109BZ31048.
  2. After successfully porting the application to PIC32CX5109BZ31048, proceed with porting it to PIC32CX5109BZ31032.
  3. Run the MPLAB® X IDE tool.
  4. In the opening window of the MPLAB X IDE, the user must locate the PIC32CX5109BZ31048 application intended for migration.
  5. Access the project properties option in MPLABX IDE. From the “default” drop-down list, select Customize.
    Figure 19-46. Customizing the PIC32CX5109BZ31032 Project Properties
  6. In the Project Properties window, perform the following steps:
    1. The user must update the device name. From the “Device:” field drop-down list, select PIC32CX5109BZ31032.
    2. From the Packs window, choose the latest version of the Device Family Pack (DFP).
      Note: The user must select the suggested DFP version.
    3. The user must opt for the latest CMSIS version. From the CMSIS folder, select 5.8.0.
    4. The user must select the recommended compiler version. From the “Compiler Toolchain:” field, select XC32 (v4.45) [C:\Program Files\Microchip\xc32\v4.45\bin].
    5. Click Apply, then click OK to ensure successful implementation of the configuration adjustments.
  7. To open the MCC for the 32-pin SoC, we need to follow these steps. To verify the availability of the BSP component, the user must navigate to the designated application directory. For example, go to H3\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\central_conn\firmware\src\config\default.
    Note: If the BSP folder is not available, skip this step and proceed directly to step 9.
    Figure 19-47. BSP Component
    1. Modifying BSP Component in .mc4 file.
      1. After finding the BSP component, the user can proceed to modify the .mc4 file to include support for the WBZ350 module.
      2. To achieve this, the user must manually edit the .mc4 file either.

      3. To manually edit the .mc4 file, perform the following steps:

      4. Navigate the location of the .mc4 file within the project.

      5. In the .mc4 file, replace all instances of the name BSP_WBZ351_Curiosity with BSP_WBZ350_Curiosity.
        Figure 19-48. .mc4 updating with BSP_WBZ350_Curiosity
      6. Save the .mc4 file.
    2. Modifying BSP Component in ble_ancs_app_default\components\BSP_WBZ351_Curiosity.yml
      1. Find and replace from BSP_WBZ351_Curiosity to BSP_WBZ350_Curiosity
      2. Save the BSP_WBZ351_Curiosity.yml
      3. Rename the BSP_WBZ351_Curiosity.yml to BSP_WBZ350_Curiosity.yml
    3. Modifying BSP Component in ble_ancs_app.X/nbproject/configurations.xml
      1. Find and replace from BSP_WBZ351_Curiosity.yml to BSP_WBZ350_Curiosity.yml
      2. Save the configurations.xml
  8. After configuring the project properties, the .mc4 file as per the requirements, run the Microchip Code Configurator (MCC) to begin the code configuration process.
    1. In the MPLAB X IDE window opening, click MCC.
      Figure 19-49. MPLAB X IDE Code Configurator
  9. The MCC now generates the project graph, which the user can view in the Project Graph tab.
    Note: The user must wait until the MCC generates the project graph.
    Figure 19-50. Project Graph
  10. The DFP will be available for the selected device, can be seen by clicking on the DFP from project graph.
    Figure 19-51. DFP Confirmation
  11. The user can verify the pin configurations in the Pin Settings tab. If the application utilizes the RGB LED, note that there will be differences in pin assignments between the WBZ351 module/ PIC32CX5109BZ31048 SoC and WBZ350 module/ PIC32CX5109BZ31032 SoC.
    Table 19-4. RGB LED Pin Differences
    RGB LED ColorWBZ350 Pin AssignmentWBZ351 Pin Assignment
    RedPB6PB0
    GreenPB7PB3
    BluePB5PB5
  12. The user must perform a force update on all components. The following are the steps to perform a force update:
    1. In the Resource Management [MCC] tab, under the “Project Resources” field, right-click on the Generate tab, then select Force Update on All.
    2. Click Generate to start the process.
    Figure 19-52. Force Update on All Components
  13. After generating the code, the MCC initiates a merging process, The merging process is not going to make changes to the application files containing customized code. However, some applications do not require certain mergers.
    Note: The merging process does not modify any application files with names beginning with app_ and does not merge the user modified files like FreeRtos_hook.c file, etc.
  14. The user must perform a thorough check to ensure the generation process is complete.
    Figure 19-53. Project Generation Complete
  15. After completing the project generation, the user must initiate the process of building the main application. In the MPLAB X IDE tool bar, click Clean and Build. From the drop-down list, select Clean and Build Main Project.
  16. Clean and build the main application, ensuring that the build is successful.
    Figure 19-54. Main Application Build Successful
  17. If you encounter any build errors related to RGB LED pin mismatches in application files (Example: app_led.h or app_led.c), ensure that the correct LED pin is specified in the code and rebuild the application.

    For example, if a WBZ351 module/ PIC32CX5109BZ31048 SoC application is configured to use the RGB LED Green pin (PB3), but you are working with a WBZ350 module/ PIC32CX5109BZ31032 SoC application, and a build error occurs due to a pin mismatch, update the RGB LED Green pin to PB7 (as used in WBZ350) in the relevant files to resolve the issue.