4.1.1.3 BLE Scanning Extended Advertisements
Getting Started with Central Building Blocks
Introduction
This document describes in detail the scanning of Extended Advertisements (ADV_EXT_IND, ADV_AUX_IND) on WBZ351 Curiosity board. For a successful scan of Extended Advertisement user needs to have a broadcaster transmitting these Advertisements. In BLE a central or observer always starts with scanning.
Usage of scan_ext_adv Application example in combination with ext_adv example will enable users to test features like long range (Coded PHY) and sending data (1M, 2M, Coded PHY) over extended advertisements
Users can run the precompiled Application Example hex file on the WBZ351 Curiosity Board and go through the steps involved in developing this Application from scratch
It is recommend to follow the examples in order, by learning the basic concepts first and then progressing to the more advanced topics.
Recommended Reading
Hardware Requirement
| Tool | Quantity |
|---|---|
| WBZ351 Curiosity Board | 2 |
| Micro USB cable | 2 |
SDK Setup
Software Requirement
Smartphone App
None
Programming the Precompiled Hex File or Application Example
Programming the hex file using MPLABX IPE
-
Precompiled Hex file is located in
"<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\scan_ext_adv\hex"folder -
For more details on the steps, go to Programming a Device
Note: Users must choose the correct Device and Tool information
Programming the Application using MPLABX IDE
-
Follow steps mentioned in of Running a Precompiled Example document
-
Open and program the Application Example "scan_ext_adv.x" located in "
<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\scan_ext_adv\firmware"using MPLABX IDE
For more details on how to find the Harmony Content Path, refer to Installing the MCC Plugin
Demo Description
This Application Example enables users to do scanning of Extended Advertisements (ADV_EXT_IND, ADV_AUX_IND PDU's). Scanning of CODED PHY (125 kbps) is enabled by default in the application. After programming the Application Example, on reset "ExtAdv Scan Enable Success" will be printed in the terminal window and if there is a broadcaster sending extended advertisements the Green LED will toggle. If this broadcaster is another WBZ351 module programmed with ext_adv example it will print the Application Data sent in Auxiliary packet - ADV_AUX_IND on TeraTerm (115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Green LED toggles denote the reception of Extended Advertisements.
Testing
Users should use another WBZ351 Curiosity Board configured as BLE Ext Adv
This section assumes that a user has already programmed the ext_adv and scan_ext_adv application on 2 WBZ351 Curiosity Boards.
Board1: WBZ351 Curiosity Board with Ext Adv Programmed
Board 2: WBZ351 Curiosity Board with Scan Ext Adv Programmed
Board1: Open TeraTerm (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Reset the board. Upon reset, "Ext Adv Enable" message is displayed on the TeraTerm.
Board 2: Open TeraTerm (Speed: 115200, Data: 8-bit, Parity: none, stop bits: 1 bit, Flow control: none). Reset the board. Upon reset, "ExtAdv Scan Enable Success" message is displayed on the TeraTerm. "Microchip" message will be displayed as soon the WBZ351 module performs an extended advertisement scan.
Developing the Application from Scratch using MPLAB Code Configurator
This section explains the steps required by a user to develop this application example from scratch using MPLABx Code Configurator
-
Create a new MCC Harmony Project. For more details, refer to 3.4 Creating a New MCC Harmony Project
Import component configuration: This step helps users setup the basic components and configuration required to develop this application. The imported file is of format .mc3 and is located in the path
"<Harmony Content Path>\wireless_apps_pic32cxbz3_wbz35\apps\ble\building_blocks\central\scan_ext_adv\firmware\scan_ext_adv.X\".For more details on how to import the component configuration , refer 13.3 Importing Existing App Example ConfigurationNote: Import and Export functionality of component configuration will help users to start from a known working setup of configuration.Accept Dependencies or satisfiers, select Yes
Verify if the Project Graph window has all the expected configuration.

Verifying Scan Configuration
- Select BLE_Stack component in project graph
Generating a Code
For more details on code generation, refer to 13.2 MPLAB Code Configurator(MCC) Code Generation.
Files and Routines Automatically Generated by the MCC
Configuration for scanning extended advertisements is autogenerated
| Source Files | Usage |
|---|---|
| app.c | Application State machine, includes calls for Initialization of all BLE stack (GAP,GATT, SMP, L2CAP) related component configurations |
app_ble\app_ble.c | Source Code for the BLE stack related component configurations, code related to function calls from app.c |
app_ble\ app_ble_handler.c | All GAP, GATT, SMP and L2CAP Event handlers |
| app_user_edits.c | User Code Change instruction |
Note: app.c is autogenerated and has a state machine based Application code sample. Users can use this template to develop their application. |
Header Files
ble_gap.h(Header Files\config\default\ble\lib\include\)- This header file contains BLE GAP functions and is automatically included in the app.c file
Function Calls
MCC generates and adds the code to initialize the BLE Stack GAP, GATT, L2CAP and SMP in APP_BleStackInit() function
APP_BleStackInit() is the API that will be called inside the Applications Initial State -- APP_STATE_INIT in app.c
User Application Development
Include
definitions.h in all the files where UART will be used to print debug information
Note:definitions.his not specific to just UART peripheral, instead it should be included in all application source files where peripheral functionality will be exercised
user action is required as mentioned 13.1 User Action
Enabling Scanning of Extended Advertisement
BLE_GAP_SetExtScanningEnable(BLE_GAP_SCAN_MODE_OBSERVER, &extScan );
Configuring LED
Add the following piece of code in GPIO_Initialize() available in - Source Files\config\default\peripheral\gpio\plib_gpio.c
GPIOB_REGS->GPIO_LAT = 0x0; /* Initial Latch Value */
GPIOB_REGS->GPIO_TRISCLR = 0x8; /* Direction Control */
GPIOB_REGS->GPIO_ANSELCLR = 0x8; /* Digital Mode Enable */Scanning Results
BLE_GAP_EVT_EXT_ADV_REPORT event is generated upon finding Adverstisements on legacy channels
// code snippet to print ext adv data
// GPIO will toggle if it can scan any EXT ADV PDU near based on BLE_GAP_SCAN_PHY chosen
GPIOB_REGS->GPIO_PORTINV = 0x08;
// length value of 19 is chosen as a filter as ext_adv example sends 19 bytes of data
// user can modify filter mechanism based on their requirements
if (p_event->eventField.evtExtAdvReport.length == 19)
{
SERCOM0_USART_Write((uint8_t *)"\r\n", 2);
SERCOM0_USART_Write(&p_event->eventField.evtExtAdvReport.advData[5], 9);
}
Users can exercise various other BLE Scanning functionalities by using BLE Stack API
For more details, refer to Getting Started with Central Building Blocks