1.1.5.5.1 DRV_I2S_BUFFER_EVENT Enumeration
Identifies the possible events that can result from a buffer add request.
Description
I2S Driver Buffer Events
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_I2S_ReadBufferAdd or DRV_I2S_WriteBufferAdd functions.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_I2S_BufferEventHandlerSet function when a buffer transfer request is completed.
C
typedef enum { DRV_I2S_BUFFER_EVENT_COMPLETE, DRV_I2S_BUFFER_EVENT_ERROR, DRV_I2S_BUFFER_EVENT_ABORT } DRV_I2S_BUFFER_EVENT;