1.1.4.8.3 DRV_WM8904_BUFFER_EVENT Enumeration
Identifies the possible events that can result from a buffer add request.
Description
WM8904 Driver Events
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_WM8904_BufferAddWrite() or the DRV_WM8904_BufferAddRead() function.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_WM8904_BufferEventHandlerSet function when a buffer transfer request is completed.
C
typedef enum { DRV_WM8904_BUFFER_EVENT_COMPLETE, DRV_WM8904_BUFFER_EVENT_ERROR, DRV_WM8904_BUFFER_EVENT_ABORT } DRV_WM8904_BUFFER_EVENT;