1.1.3.8.1 DRV_GENERICCODEC_BUFFER_EVENT Type
Identifies the possible events that can result from a buffer add request.
Description
Generic Codec Driver Events
This enumeration identifies the possible events that can result from a buffer add request caused by the client calling either the DRV_GENERICCODEC_BufferAddWrite() or the DRV_GENERICCODEC_BufferAddRead() function.
Remarks
One of these values is passed in the "event" parameter of the event handling callback function that the client registered with the driver by calling the DRV_GENERICCODEC_BufferEventHandlerSet function when a buffer transfer request is completed.
C
typedef enum DRV_GENERICCODEC_BUFFER_EVENT@1 DRV_GENERICCODEC_BUFFER_EVENT;