1.1.1.4.10 DRV_AK4953_SamplingRateGet Function
uint32_t DRV_AK4953_SamplingRateGet(DRV_HANDLE handle)
Summary
This function gets the sampling rate set on the DAC AK4953.
Description
This function gets the sampling rate set on the DAC AK4953.
Preconditions
The DRV_AK4953_Initialize routine must have been called for the specified AK4953 driver instance.
DRV_AK4953_Open must have been called to obtain a valid opened device handle.
Parameters
Parameters | Description |
---|---|
handle | A valid open-instance handle, returned from the driver's open routine |
Returns
None.
Remarks
None.
Example
uint32_t baudRate; _\/\/ myAK4953Handle is the handle returned \/\/ by the DRV_AK4953_Open function._ baudRate = DRV_AK4953_SamplingRateGet(myAK4953Handle);
C
uint32_t DRV_AK4953_SamplingRateGet(DRV_HANDLE handle);