1.1.5.4.5 DRV_I2S_ProgrammableClockSet Function
bool DRV_I2S_ProgrammableClockSet(DRV_HANDLE handle, uint8_t pClkNum, uint8_t div2);Summary
Set the Programmable Clock
Description
Set the Programmable Clock ignoring glitch control
Preconditions
None.
Returns
True - if the function was successful
False - if a timeout occurred (no transitions seen)
Remarks
None.
Example
_// myI2SHandle is the handle returned_ _// by the DRV_I2S_Open function._ DRV_I2S_ProgrammableClockSet(myI2SHandle, 2, 7);
C
bool DRV_I2S_ProgrammableClockSet(DRV_HANDLE handle, uint8_t pClkNum, uint8_t div2);