1.1.5.4.4 DRV_I2S_ClockGenerationSet Function
bool DRV_I2S_ClockGenerationSet(DRV_HANDLE handle, uint8_t div, uint8_t mul, uint8_t div2);Summary
Set the clock(PLLA and I2SC GCLK clock) generation values
Description
Set the clock(PLLA and I2SC GCLK clock) generation values
Preconditions
None.
Returns
True - if the function was successful
False - if a timeout occurred (no transitions seen)
Remarks
None.
Example
_// myI2SHandle is the handle returned_ _// by the DRV_I2S_Open function._ DRV_I2S_ClockGenerationSet(myI2SHandle, 2, 40, 5);
C
bool DRV_I2S_ClockGenerationSet(DRV_HANDLE handle, uint8_t div, uint8_t mul, uint8_t div2);