6 Modify file system details in menuconfig to boot from NAND Flash
- Enter the following command to modify
the
configurations:
$ make menuconfigThe configuration window opens.
- From the menu, select Filesystem
images and press Enter.
- In the Filesystem
images window, ensure the ubi image containing an ubifs root
filesystem checkbox is enabled. If not, select it and press ‘Y’ to
enable.
- In the Filesystem
images window, select physical eraseblock size and press
Enter.
- Update the physical
eraseblock size to 0x40000 and press Enter. The physical
erase block size is the NAND Flash block size in bytes.
- In the Filesystem images window, select sub-page size and press Enter.
- Update the sub-page
size to 4096 and press Enter. Some NAND Flash devices support
sub-pages,and some do not. Those that do not must be updated with the actual
page size as the sub-page size.
- In the Filesystem images window, ensure ubifs root filesystem is enabled. If not, select it and press ‘Y’ to enable.
- In the Filesystem images window, select logical eraseblock size and press Enter.
- Update the logical
eraseblock size to 0x3E000 and press Enter. The logical
eraseblock size is calculated by subtracting two pages from the physical
eraseblock size (LEB = PEB – 8192). Each of the two pages contains an EC
header and a VID header.Note: This calculation is applicable only for a NAND Flash which does not support sub-pages. For a NAND Flash supporting sub-pages, the calculation varies with the sub-page size.
- In the Filesystem images window, select minimum I/O unit size and press Enter.
- Update the minimum I/O
unit size to 0x1000 and press Enter. The minimum I/O unit
size is equivalent to the NAND Flash device page size.
- In the Filesystem images window, select maximum logical eraseblock count and press Enter.
- Update the maximum logical
eraseblock count to 2048 and press Enter. The maximum logical
eraseblock count is the total number of blocks of the NAND Flash
device.

- Press ESC twice to exit the menu.
- In the Filesystem
images window, ensure the ubi image containing an ubifs root
filesystem checkbox is enabled. If not, select it and press ‘Y’ to
enable.
- Select Exit and press
Enter.
- Click Yes.

- Click Yes.