Introduction
This document describes how to boot Linux on a SAM9X60 device from a NAND Flash memory.
The device can boot from any of the external non-volatile memories (NVM) available on the board, such as an SD card, e.MMC, QSPI, SPI or NAND Flash memory. To boot from a NAND Flash memory, at91bootstrap, u-boot, the Linux Kernel and the root file system must be flashed into the NAND Flash memory. This document explains how to configure, build and program files on the SAM9X60.