8 Final Build
After all required changes are made, the build can be performed.
- Navigate to the buildroot-mchp
directory:
$ cd buildroot-mchp - Build the at91bootstrap with the
following command:
$ makeThe build will take a few hours to complete.
- Once the build is complete, navigate to buildroot-mchp/output/Images.
- Verify that the following files
are generated:
- at91bootstrap.bin
- u-boot.bin
- at91-sam9x60_curiosity.dtb
- zImage
- rootfs.ubi