6 Migrating MRF24Wx to ATWINC15x0 using Harmony Framework
This section describes how to migrate from the MRF24WX module to the ATWINC15x0 module for the user who has the Wi-Fi
solution in Harmony framework. The user needs to use the Microchip MPLAB Harmony
configuration (MHC) for seamless migration.Figure 6-1. Setup Procedure
The user must disconnect the SPI bus,
Reset, Chip enable and interrupt lines from the MCU to MRF24WN, then connect the
same lines to the ATWINC15x0 module.
Note: The user
does not need to perform the application or driver changes manually.
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.