3.6 Pin Configuration

Some pins of the LAN8670/1/2 may take on multiple functions depending on the device and mode. The functionality of five pins of the LAN8670 varies depending upon the device mode set by the MODE[1:0] Configuration Straps. Table   1 shows the functionality assigned to these pins based on the configured device mode.

Table 3-13. LAN8670 Device Mode Pin Configuration
MIISC-MIIRMII

Pin 11

(TXER/ACMA)

TXER1

ACMA

ACMA

Pin 12

(TXCLK/RXPI)

TXCLK2

RXPI

RXPI

Pin 15

(CRS)

CRS

CRS

Not Used

Pin 17

(RXCLK/SMCLK/WAKE_OUT)

RXCLK

SMCLK

WAKE_OUT

Pin 20

(RXDV/CRSDV)

RXDV

RXDV

CRSDV

Note:
  1. GPIO0 may be used for ACMA
  2. GPIO0 may be used for RXPI

The GPIO0 pin is a multipurpose pin that can be configured as desired for multiple uses. This feature is useful for enabling specific features that would not otherwise be available for a specific device package or configuration. For example, Time Sensitive Networking (TSN) is supported through the ability to assert output signals when packets matching a specific pattern are transmitted and/or received. The GPIO0 pin may be configured as a Transmit Packet Indication (TXPI), Receive Packet Indication (RXPI), or Receive/Transmit Packet Indication (RXTXPI) output, as needed. Additionally, GPIO0 may be configured as an Application Controlled Media Access (ACMA) input pin.

The GPIO0 pin functionality is configured by writing to the GPIO0 Signal Select (GPIO0SS) field of the Pin Control (PINCTRL) register. The GPIO0 Signal Select should be configured prior to configuring and enabling the underlying Packet Pattern Matching or Application Controlled Media Access blocks.

Valid configurations for the GPIO0 pin depend on the device in use and its operating mode. When a dedicated native pin is available, this pin must be used for the provided function rather than the GPIO0 pin. Table 3-14 below shows the valid configurations for the GPIO0 pin. When a pin number is shown, this is an invalid configuration for the GPIO0 Signal Select and the designated dedicated pin must be used instead.

For devices of revision D0 and onward, the configuration of the GPIO0 can be overwritten by the Link Status Control (LSCTL) Register if the Link Status Pin Select (LSPSEL) field is configured to use the GPIO0 pin.

Table 3-14. GPIO0 Signals
LAN8670LAN8671LAN86721
GPIO0SSSignalMIISC-MIIRMIIRMIIMII
00RXPI✔Pin 12Pin 12✔Pin 14
01TXPI✔✔✔✔✔
10RXTXPI✔✔✔✔✔
11ACMA✔Pin 11Pin 11✔Pin 13
Note:
  1. LAN8672 Revision C2, only.

Because the LAN8670 supports all operating modes, those being Media Independent Interface (MII), Single-Clock MII (SC-MII), and Reduced Media Independent Interface (RMII), it is important to know in which mode the device will be operated in. In MII mode, GPIO0 can be configured to any of the four possible functions. However, in SC-MII and RMII modes, it is limited to only be configured as TXPI or RXTXPI functionality.

For the LAN8671, GPIO0 may again fulfill any of the four possible configurations. To be noted here, the LAN8671 is only operated in RMII mode.

For the LAN8672, revision C2, GPIO0 may again only be configured as TXPI or RXTXPI, since this device only operates in MII mode.