3.6.1.3 Provisioning Webpage
The following table provides the command syntax for firmware upgrade (provisioning webpage).
| Command Syntax | Upgrade_1500_provisioning webpage/ Upgrade_3400_provisioning_webpage | ||||
|---|---|---|---|---|---|
| X | X refers to Antenna
| ||||
| Example | Upgarde_1500_provisioning_webpage ATWINC1500 webpage update | ||||
The following figure shows the example of firmware upgrade (provisioning webpage).

Note: ASF has the latest firmware. See
Firmware upgrade folder in MCHPRT2 package, for information on how to add the upgrade
file into MCHPRT2 tool folder.
Important: Before the
Firmware upgrade, update the Firmware file in the following folder:
- ..\MCHPRT\upgrade_1500\firmware\firmware (for ATWINC1500)
- ..\MCHPRT\upgrade_3400\firmware\firmware (for ATWINC3400)