9.2.2 Writing to a ROM Zone Register
A ROM Zone register can only be written to a logic ‘1’,
which will set the corresponding memory zone to a ROM state. Once a ROM Zone register has
been written, it can never be altered again.
To write to a ROM Zone register, the host must send a Start condition,
followed by the device address byte with the opcode of 0111b (7h)
specified, along with the appropriate client address combination and the
Read/Write bit set to a logic ‘0’. The device
will return an ACK. After the device address byte has been sent, the AT21CS01/AT21CS11 will return an ACK.
Following the device address byte is an 8-bit ROM Zone register address byte. The address sent to the device must match one of the ROM Zone register addresses specified in Table 9-2. After the ROM Zone register address has been sent, the AT21CS01/AT21CS11 will return an ACK.
After the AT21CS01/AT21CS11 has sent the ACK, the
host must send an FFh data byte to set the appropriate ROM Zone register to the logic
‘1’ state. The device will then return an ACK and, after a Stop
condition is executed, the device will enter a self-time internal write cycle, lasting
tWR. If a Stop condition is sent at any other point in the
sequence, the write operation to the ROM Zone register is aborted. The device will not
respond to any commands until the tWR time has completed. This
sequence is depicted in Figure 9-2.