4.1.3.1 Data Input Bit Frames
A data input bit frame can be used by the host to transmit either a logic
‘0’ or logic ‘1’ data bit to the AT21CS01/AT21CS11. The input bit frame is initiated when the host drives the SI/O
line low. The length of time that the SI/O line is held low will dictate whether the host
is transmitting a logic ‘0’ or a logic ‘1’ for that bit
frame. For a logic ‘0’ input, the length of time that the SI/O line must
be held low is defined as tLOW0. Similarly, for a logic
‘1’ input, the length of time that the SI/O line must be held low is
defined as tLOW1.
The AT21CS01/AT21CS11 will sample the state of
the SI/O line after the maximum tLOW1 but prior to the minimum
tLOW0 after SI/O is driven below the VIL threshold to determine if the data input is a logic ‘0’ or a
logic ‘1’. If the host is still driving the line low at the sample
time, the AT21CS01/AT21CS11 will decode that bit frame as a logic
‘0’ as SI/O will be at a voltage less than VIL. If the host has already released the SI/O line, the AT21CS01/AT21CS11 will see a voltage level greater than or equal to VIH because of the external pull-up resistor, and that bit frame
will be decoded as a logic ‘1’. The timing requirements for these
parameters can be found in AT21CS01/AT21CS11 AC
Characteristics.
A logic ‘0’ condition has multiple uses in the I2C emulation sequences. It is used to signify a
‘0’ data bit, and it is also used for an Acknowledge (ACK) response.
Additionally, a logic ‘1’ condition is used for a No Acknowledge (NACK)
response in addition to the nominal ‘1‘ data bit.
Figure 4-2 and Figure 4-3 depict the logic ‘0’ and logic
‘1’ input bit frames.
0’ Input Condition Waveform1’ Input
Condition Waveform