4.1.3.4 Data Output Bit Frame
A data output bit frame is used when the host is to receive communication back from the AT21CS01/AT21CS11. Data output bit frames are used when reading any data out as well as any ACK or NACK responses from the device. Just as in the input bit frame, the host initiates the sequence by driving the SI/O line below the VIL threshold, which engages the internal timing generation circuit of the AT21CS01/AT21CS11.
Within the output bit frame is the critical timing parameter, tRD, which is defined as the amount of time the host must continue to drive the SI/O line low after crossing the VIL threshold to request a data bit from the AT21CS01/AT21CS11. Once the tRD duration has expired, the host must release the SI/O line.
If the AT21CS01/AT21CS11 responds with a logic
‘0’ (for either a ‘0’ data bit or an ACK response), it
will begin to pull the SI/O line low concurrently during the tRD window and continue to hold it low for a duration of tHLD0, after which it will release the line to be pulled back up to VPUP (see Figure 4-6). Thus,
when the host samples SI/O within the tMRS window, it will see
a voltage less than VIL and decode this event as a
logic ’0’. By definition, the tHLD0 time is
longer than the tMRS time and therefore, the host is ensured to
sample while the AT21CS01/AT21CS11 is still driving the SI/O line
low.
0’ Data Output Bit Frame WaveformIf the AT21CS01/AT21CS11 intends to respond with
a logic ‘1’ (for either a ‘1’ data bit or a NACK
response), it will not drive the SI/O line low at all. Once the host releases the SI/O line
after the maximum tRD has elapsed, the line will be pulled up
to VPUP. Thus, when the host samples the SI/O line within the
tMRS window, it will detect a voltage greater than VIH and decode this event as a logic ‘1’.
The data output bit frame is shown in greater detail in Figure 4-7.
1’ Data Output Bit Frame Waveform