6 Appendix 2: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under directory TCL_Scripts. If required, the design flow can be reproduced from Design Implementation till generation of job file.
To run the TCL, follow the steps:
- Launch the Libero software.
- Select
- Click Browse and select
script.tclfrom the downloaded TCL_Scripts directory. - Click Run.
After successful execution of TCL script, Libero project is created within TCL_Scripts directory.
For more information about TCL scripts, refer to mpf_an5102_v2023p1_df/TCL_Scripts/readme.txt.
See the Libero® SoC TCL Command Reference Guide for more details on TCL commands. Contact Technical Support for any queries encountered while running the TCL script.