7 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

RevisionDateDescription
A08/2023The following is the list of changes in revision A of the document:
  • The document was migrated to the Microchip template.
  • The document number was updated to DS00005102 from 50200757.
  • The document was updated for Libero SoC v2023.1 release.
8.0—The following is a summary of the changes made in this revision.
  • Updated the document for Libero SoC v12.2.
  • Removed the references to Libero version numbers.
7.0—The document was updated for Libero SoC v12.0 release.
6.0—The document was updated for Libero SoC PolarFire v2.2 release.
5.0—The document was updated for Libero SoC PolarFire v2.1 release.
4.0—The following is a summary of the changes made in this revision.
  • The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v2.0 release.
  • The design requirements were updated. For more information, see Design Requirements.
  • Details about the demo design, including the hardware implementation block diagram, were updated. For more information, see Demo Design.
  • Clocking Structure diagram was added. For more information, see Figure   1.
  • A new section which details the reset structure of the design is added. For more information, see Reset Structure.
  • Information about simulating the design was updated. For more information, see Simulating the 10GBASE-R Ethernet SyncE Loopback Design.
3.0—The following is a summary of the changes made in this revision.
  • The document was updated to include features and enhancements introduced in the Libero SoC PolarFire v1.1 SP1 release.
  • Hardware requirements were added, and software requirements were updated to include Spirent TestCenter and FlashPro. For more information, see Design Requirements.
  • Information about how to program the device was added. For more information, see Appendix 1: Programming the Device Using FlashPro Express.
  • Information about how to run the hardware reference design was added. For more information, see Running the Demo.
2.0—The following is a summary of the changes made in this revision.
  • The document was updated for Libero SoC PolarFire v1.1 release.
  • Information about resource utilization was added. For more information, seeResource Utilization.
1.0—The first publication of this document.