5.4.2.2 Unconfigure a NVMe Drive from Physical Device Level

To unconfigure a configured NVMe drive which is not part of an array:
  1. Select a desired configured device based on label.
  2. On the ribbon, in the Physical Device group, click Set Properties.

    The Set Properties window opens.

  3. Select Unconfigured option from the XLR Configuration State drop-down list.
  4. Click OK.
Note: Once you Configure/Unconfigure the NVMe drives, a reboot is necessary for any effect to take place. Until the reboot, no configuration change operations can be performed on the controller.