5.4.2.1 Configure a NVMe Drive from Physical Device Level

To configure the unconfigured NVMe drive:
  1. Select the unconfigured device based on the PCIe address under the Unconfigured Devices group node.
  2. On the ribbon, in the Physical Device group, click Set Properties.

    The Set Properties window opens.

  3. Select Configured option from the XLR Configuration State drop-down list.
  4. Specify a label in ASCII format that does not include spaces and has a maximum of eight characters. This label is further used to identify each NVMe drive.
  5. Click OK.