5.4.2.2 Unconfigure a NVMe Drive from Physical Device Level
To unconfigure a configured NVMe drive which is not part of an array:
- Select a desired configured device based on label.
- On the ribbon, in
the Physical Device group, click Set
Properties.

The Set Properties window opens.
- Select
Unconfigured option from the XLR
Configuration State drop-down list.

- Click OK.