2.1.2 Debugger/Programmer Selection

By default, the external debugger is connected to the programming pins (PGEC2 and PGED2) of the WFI32E01PC/WFI32E03PC module. The following table lists the details of the debugger/programmer selection using the J301 header.

Note: For the jumper connections, refer to the PIC32 WFI32E Curiosity Board User’s Guide (DS50003028).
Important: Use an external debugger such as MPLAB® ICD 5, MPLAB® PICkit™ 5, or MPLAB® Snap for the best programming and debugging experience.
The PIC32 WFI32E Curiosity Board has an on-board debugger (PKOB3) based on the PIC24FJ256GB106 MCU. The on-board debugger enables the user to power, program and debug through the micro-B USB connector (J302).
Table 2-2. Debugger/Programmer Selection
Header Position (J301(1))Debugger Used Description
Pins 1-2 and 3-4 shortedOn-boardSelects the on-board debugger.
Pins 1-2 and 3-4 openExternalSelects the external debugger (for more details, refer to ICSP Header).
Note:
  1. For the jumper connections, refer to the PIC32 WFI32E Curiosity Board User’s Guide (DS50003028).