4 Appendix 2: Running the TCL Script
(Ask a Question)TCL scripts are provided in the design files folder under the directory
HW. If required, the design flow can be reproduced from Design
Implementation to the job file generation.
To run the TCL, perform the following steps:
- Launch the Libero software.
- Click .
- In the downloaded
HWdirectory, selectscript.tcland click Browse. - Click Run.
After successful execution of TCL script, the Libero project is created within
HW directory. For more information about TCL scripts, see
mpf_an4682_df/HW/TCL_Scripts_readme.txt.
For more details on TCL commands, see Tcl Commands Reference Guide . Contact Technical Support for any queries about running the TCL script.