5 Revision History

The revision history describes the changes that were implemented in the document. The changes are listed by revision, starting with the most current publication.

Table 5-1. Revision History
RevisionDateDescription
C07/2025The following is the list of changes in revision C of the document:
B05/2024The following is the list of changes in revision B of the document:
  • In the Demo Design section as follows:
    • Updated the temperature channel's output value
    • Added the calculation part which illustrates how to calculate temperature and voltage output value
A07/2022The following is the list of changes in revision A of the document:
  • The document was migrated to the Microchip template
  • The document number was updated to DS00004682A from 50200852
  • The document ID was updated to AN4682 from DG0852
  • Updated the Figure 1-2
  • Removed Resource Utilization section
3.0—

The following is a summary of the changes made in this revision.

Added Appendix 2: Running the TCL Script.

Updated Figure 2, page 4.

2.0—

The following is a summary of the changes made in this revision.

Updated the document for Libero SoC v12.2.

Removed the references to Libero version numbers.

1.0—The first publication of this document.