3 Appendix 1: Programming the Device Using FlashPro Express
(Ask a Question)To program the PolarFire device with the .job programming file
using FlashPro Express. The .job file is available at the following
design files folder location: mpf_an4682_df\Programming_files
To program the device, perform the following steps:
- Ensure that the jumper settings on the board are the same as listed in Table 1-4.Important: The power supply switch must be switched off while making the jumper connections.
- Connect the power supply cable to the J9 connector on the board.
- Connect the USB cable from the Host PC to the J5 (FTDI port) on the board.
- Power the board using the SW3 slide switch.
- On the host PC, start the FlashPro Express software.
- To create a new job project on the Project menu, click New or New Job Project from FlashPro Express Job.
- In the New Job Project from FlashPro
Express Job dialog box, perform the following steps:
- Programming job file: Click
Browse, navigate to the location where the
.jobfile is located and select the file. The default location is: <download_folder>\mpf_an4682_df\Programming_files. - FlashPro Express job project location: Select Browse and navigate to the location where you want to save the project.
Figure 3-1. New Job Project from FlashPro Express Job - Programming job file: Click
Browse, navigate to the location where the
- Click OK. The required
programming file is selected and ready to be programmed in the device. The FlashPro
Express window appears. Verify that a programmer number appears in the Programmer
field. If it does not, verify the board connections and click
Refresh/Rescan Programmers.
Figure 3-2. Programming the Device - To program the device, click RUN. When the device is
programmed successfully, a RUN PASSED status is displayed, as
shown in the following figure. To run the TVS demo, see Running the Demo.
Figure 3-3. FlashPro Express-RUN PASSED - Close FlashPro Express, click .