1 PolarFire FPGA Temperature and Voltage Sensor
(Ask a Question)This demo highlights the TVS feature of the PolarFire® using a UART-based application (GUI). The demo design continuously pumps the data from TVS channels to UART, displayed on the GUI. This demo design also shows how to simulate the TVS feature of the PolarFire device.
The demo design can be programmed using one of the following options:
- Using the job file: To program the device using the job file provided along with the design files, see Appendix 1: Programming the Device Using FlashPro Express.
- Using Libero® SoC: To program the device using Libero SoC, see Running the Demo section. Use this option when the demo design is modified.