32.2.6 ADC Conversion Procedure (Basic Mode)
This is an example procedure for using the ADC to perform an Analog-to-Digital Conversion:
- Configure Port:
- Disable pin output driver (refer to the TRISx register)
- Configure pin as analog (refer to the ANSELx register)
- Configure the ADC module:
- Configure ADC interrupt (optional):
- Clear ADC interrupt flag
- Enable ADC interrupt
- Enable global interrupt (GIE bit)(1)
- If ADACQ !=
0, software must wait the required acquisition time(2). - Start conversion by setting the GO bit.
- Wait for ADC conversion to complete by
one of the following:
- Polling the GO bit
- Waiting for the ADC interrupt (if interrupt is enabled)
- Read ADC Result.
- Clear the ADC interrupt flag (if interrupt is enabled).
Note:
- With global interrupts disabled (GIE
=
0), the device will wake from Sleep, but will not enter an Interrupt Service Routine. - Refer to the ADC Acquisition Requirements section for more details.
ADC Conversion (Single-Ended Input)
/*This code block configures the ADC
for polling, VDD and VSS references,
ADCRC oscillator.
Conversion start & polling for completion
are included.
*/
void main()
{
initializeSystem(); //System Initialize
//Setup ADC
ADCON0bits.FM = 1; //Right justify
ADCON0bits.CS = 1; //ADCRC Clock
ADPCH = 0x00; //RA0 is positive input
TRISAbits.TRISA0 = 1; //Set RA0 to input
ANSELAbits.ANSELA0 = 1; //Set RA0 to analog
ADACQ = 32; //Set acquitisition time
ADCON0bits.ON = 1; //Turn ADC On
while (1)
{
ADCON0bits.GO = 1; //Start conversion
while (ADCON0bits.GO); //Wait for conversion done
resultHigh = ADRESH; //Read result
resultLow = ADRESL; //Read result
}
}