2.7.3 Software Requirements
The following are the software requirements:
- Microchip Bluetooth Low Energy Virtual Sniffer Tool – Microchip provides a Bluetooth Low Energy Virtual Sniffer Tool package that contains the necessary files, including a Python executable to run the virtual sniffer functionality. For downloading the Bluetooth Low Energy Virtual Sniffer Tool, go to the Bluetooth Low Energy Virtual Sniffer Tool (v1.00).
- For downloading the Wireless Protocol
Suite, go to the Wireless Protocol Suite (v2.35 or later) from Teledyne LeCroy.
- -wps-2.35_22.4.29031.29650 or the later version
Note: In this user guide, for testing the virtual sniffer, the software version used is - wps-2.35_22.4.29031.29650.