16.6.2.1 Initialization
The following bits are enable-protected,
meaning that they can only be written when the RTC is disabled
(CTRL.ENABLE=0):
- Operating Mode bits in the Control register (CTRL.MODE)
- Prescaler bits in the Control register (CTRL.PRESCALER)
- Clear on Match bit in the Control register (CTRL.MATCHCLR)
- Clock Representation bit in the Control register (CTRL.CLKREP)
The following register is enable-protected:
- Event Control register (EVCTRL)
Any writes to these bits or registers when
the RTC is enabled or being enabled (CTRL.ENABLE=1) will be discarded.
Writes to these bits or registers while the RTC is being disabled will be completed after
the disabling is complete.
Enable protection is denoted by the "Enable-Protected" property in the register description.
- RTC operation mode must be selected by writing the Operating Mode bit group in the Control register (CTRL.MODE)
- Clock representation must be selected by writing the Clock Representation bit in the Control register (CTRL.CLKREP)
- Prescaler value must be selected by writing the Prescaler bit group in the Control register (CTRL.PRESCALER)
The frequency of the RTC clock (CLK_RTC_CNT) is given by the following formula:
The frequency of the generic clock, GCLK_RTC, is given by fGCLK_RTC, and fCLK_RTC_CNT is the frequency of the internal prescaled RTC clock, CLK_RTC_CNT.