7.2 ATWILC1000 and ATWILC3000 Firmware Binaries
- Add the ATWILC1000 firmware
wilc1000_wifi_firmware.binto the/lib/firmware/mchp/directory. - Add the ATWILC3000 Wi-Fi firmware,
wilc3000_wifi_firmware.binto the/lib/firmware/mchp/directory. - Add the ATWILC3000 Bluetooth®
firmware,
wilc3000_ble_firmware.binto the/lib/firmware/mchp/directory.
Note: The firmware is available at https://github.com/linux4wilc/firmware.
The files can be transferred into the SAMA5D4 platform using any of the following methods:
- Ethernet
- ZMODEM