7.2.2 Adding Files using ZMODEM
The ZMODEM file transfer protocol also can be used to transfer the files.
In Teraterm, change the target location directory using the following
command:
$ cd Target_locationExecute the ZMODEM command using the following
command:
$ rzIn Teraterm, from the File menu, choose
Transfer > Send, then browse and select the
desired file.