- When using interrupt priority
                    levels, set IPEN and then select the user-assigned priority level for the
                    interrupt source by writing the control bits in the appropriate IPRx control
                        register.
Important: At a device Reset, the IPRx registers are initialized such
                        that all user interrupt sources are assigned to high priority.
 
                - Clear the Interrupt Flag Status
                    bit associated with the peripheral in the associated PIRx STATUS register.
 
                - Enable the interrupt source by
                    setting the interrupt enable control bit associated with the source in the
                    appropriate PIEx register.
 
                - If the vector table is used
                    (MVECEN = 
1), then set up the start address for the Interrupt
                    Vector Table using IVTBASE. See the Interrupt
                        Vector Table Contents section for more details. 
                - Once IVTBASE is written to, set
                    the interrupt enable bits in INTCON0. 
 
                - An example of setting up
                    interrupts and ISRs can be found below.
 
            
            
         
        Setting Up Vectored Interrupts
                Using XC8
            
            
void __interrupt(irq(IRQ_SW), base(0x3008)) SW_ISR(void)
{
    PIR0bits.SWIF = 0;    
    LATCbits.LATC0 ^= 1;    
}
void __interrupt(irq(default), base(0x3008)) DEFAULT_ISR(void)
{
    
}
void INTERRUPT_Initialize (void)
{
    INTCON0bits.GIEH = 1;    
    INTCON0bits.GIEL = 1;    
    INTCON0bits.IPEN = 1;    
    PIE0bits.SWIE = 1;     
    PIE0bits.HLVDIE = 1;     
    IPR0bits.SWIP = 0;     
    
    IVTBASEU = 0x00;          
    IVTBASEH = 0x30;          
    IVTBASEL = 0x08;
}