33.1.1 ADC Input Configuration
The ADC Input Configuration (IC) bit is used to determine whether the ADC uses both positive and negative input channels in differential operations or only the positive input channel in single-ended operations.
When IC is set (IC = 1
), the ADC operates in Differential mode. In
Differential mode, the ADC calculates the difference between a positive analog input
signal and a negative analog input signal with respect to the ADC reference voltage
(VREF), and the conversion result may be a positive or negative value.
The positive input signal is selected by the ADC Positive Channel Selection (ADPCH)
register, and the negative input signal is selected by the ADC Negative Channel
Selection (ADNCH) register. The ADC reference voltage (VREF) is the
difference between the ADC Positive Voltage Reference (VREF+) input
and the ADC Negative Voltage Reference
(VREF-) input.
When IC is clear (IC = 0
), the ADC operates in Single-Ended mode. In
Single-Ended mode, the ADC converts the positive input signal with respect to
VREF, and the conversion result will be a positive value. The positive
input is selected by ADPCH, similar to Differential mode; however, in Single-Ended mode,
ADC hardware ignores any negative input selections selected by ADNCH. In Single-Ended
mode, VREF is the difference between VREF+ and
VSS.