4.1.1.2 Booting from a QSPI Memory
Before enabling boot from a QSPI memory, the configuration described below is mandatory.
- Go to the SAM-BA installation
path.
<user>\sam-ba_v3.7-win32\sam-ba_v3.7-rc2-win32\qml\SAMBA\Device\SAMA5D29\SAMA5D29.qml
- Open the SAMA5D29.qml and add the config structure below to the
file.
config {// QSPI1, I/O Set 2, 66MHzqspiflash {instance: 1ioset: 2freq: 66}}
To configure and enable a boot from a QSPI memory, send the following commands:
- Enable boot from QSPI memory in
the Boot Configuration Word.
sam-ba -p serial -d sama5d29 -a bootconfig -c writecfg:bureg0:QSPI1_IOSET2,EXT_MEM_BOOT

sam-ba -p serial -d sama5d29 -a bootconfig -c writecfg:bscr:bureg0,valid
Note: To enable boot on another Flash memory than the default SDMMC, the Fuse EXT_MEM_BOOT must be set (NAND, QSPI, SPI). The ROM code will then attempt to boot on all the Flash memories indicated in the Boot Configuration Word. Erase the QSPI Flash.
sam-ba -p serial -d sama5d29 -a qspiflash -c erase

- Write and verify the bootstrap
file in QSPI Flash.
sam-ba -p serial -d sama5d29 -a qspiflash -c writeboot:boot.bin -c verifyboot:boot.bin

- Write and verify the app file in
QSPI Flash.
sam-ba -p serial -d sama5d29 -a qspiflash -c write:harmony.bin:0x40000 -c verify:harmony.bin:0x40000

- Reset to boot from QSPI
memory.
sam-ba -p serial -d sama5d29 -a reset