4.1 RTL Simulation Mode
(Ask a Question)RTL simulation mode simulates the XCVR block from the fabric interface to the serial I/O interface. RTL simulation mode is available for all of the XCVR modes. This mode supports all of the protocol communication layers, including the physical layer, and provides accurate cycle simulation for the design. Using RTL simulation, however, experiences some run-time penalties. As the IP user block is off-chip, it must be connected to the user design in the top-level test bench. It is the user’s responsibility to provide the model for the off-chip IP that can communicate with the XCVR block in the same protocol used by the XCVR block when using this mode. Post-synthesis simulation is available with PF_XCVR_ERM designs when configured with both ERM OFF and ON.
To minimize simulation time, certain peripherals in the transceiver do not have full behavioral models. These models are replaced with memory models that output a message indicating when the memory locations inside the peripheral are accessed. The memory models are created by using register information that is generated by Libero. The XCVR register data is found at <Libero Project>\component\work\<top_level>\<xcvr_component_name>. The peripheral signals do not toggle based on any writes to registers, or react to any signal inputs on the protocol pins.
Using RTL simulation mode, the FPGA designer can have an off-chip verification IP model that communicates with the transceiver. For example, if the design uses a 8b10b XCVR block, the FPGA designer must have a 8b10b verification IP off-chip block to communicate with the XCVR block using the required protocol. When the IP user block is off-chip, it must be connected to the design in the top-level testbench.