| Revision 9.0 | 5/21 | The following is a summary of the changes in this revision.- Information about incremental DFE calibration was added. See DFE Calibration.
- Information about Enhanced Receiver Management was updated.
- Information about Transceiver Reference Clock Interface was updated.
- Information about spread spectrum was updated. See Table 28.
- Information about PIPE Port List and PMA Port List was updated.
- Information about Loss of Signal Detect (LOS) was added.
- Information about PMA and PCS Resets was updated.
- Information about Transceiver Reference Clock Configurator was updated.
- Information about Dynamic Reconfiguration Interface was updated.
- Information about Jitter Attenuator was updated.
- Information about Transceiver Initialization was updated.
- Information about Libero Generated Files was updated.
|
| Revision 8.0 | 9/20 | The following is a summary of the changes in this revision.- Information about 8b10b Data Path Interface, 8b10b Bit and Octet Sequencing, and 8b10b System Registers was added.
- Information about 64b6xb Data Path Interface, 64b6xb System Registers, 64b66b Receiver, 64b66b Transmit, 64b67b Transmit, and 64b67b Receive was added.
- Information about None_DFE (Static DFE) was updated. See Enhanced Receiver Management.
- Information about LANE#_CLK_REF port name was added. See Table 7, Table 11, Table 12, and Table 13.
- Information about Table 21 was updated.
- Information about DFE Coefficients was added.
- Information about AC/DC Coupled Connection was updated.
- Information about Table 39 was updated.
- Information about Design for Protocols and Unused Transceiver Pins was updated.
- Information about Half-Duplex Mode was updated.
- Information about Receive Input Buffer was updated.
|
| Revision 7.0 | 4/20 | The following is a summary of the changes in this revision.- Information about physical constraint instances was updated. See Table 34.
- Information about TX and RX interface clock was updated. See Table 16.
- Information about Enhanced Receiver Management was updated.
|
| Revision 6.0 | 1/20 | The following is a summary of the changes in this revision.- Information about capability to support switching between two TXPLLs or two CDR REFCLKs through the DRI interface was added. See Transceiver Interface Configurator.
- Information about LiteFast was updated. See Table 1.
- Information about PCS/FPGA Fabric Interface was added.
- Information about new latency was updated. See Table 15.
- Information about Transceiver Data Path Latency was added.
- Information about footnote was updated. See Table 21.
- Information about PCS Rate Switch Between 8b10b and 64b66b Mode for CPRI was added.
- Information about MPF500 Transceiver and Transmit PLL Layout was updated. See Figure 53.
- Information about JA PLL settings for each preset was added. See Jitter Attenuator.
- Information about Transceiver Modes was added.
- Information about PMA and PCS Resets was updated.
- Information about Custom Protocol Settings was added.
- Information about Table 7, Table 11, Table 12, and Table 13 was updated.
|
| Revision 5.0 | 3/19 | The following is a summary of the changes in this revision.- Information about SATA sub-mode was removed from PIPE.
- Information about RX_IDLE was updated. See Table 7, Table 11, and Table 13.
- Information about LANE#_TX_WCLK input pin was added. See PCS/FPGA Fabric Interface.
- Information about Transceiver Clock Regions was added.
- Information about Reference Clock Disruptions was added.
- Information about Jitter Attenuator was added.
- Information about REFCLK input pins were updated. See Reference Clock Input Pins.
- Information about PMA and PCS Resets was added.
- Information about the interface clocks for the Transceiver PLL was updated. See Table 32.
- Information about Enhanced Receiver Management was added.
- Information about PIPE Interface Compliance Exceptions was added.
|
| Revision 4.0 | 10/18 | The following is a summary of the changes in this revision.- Updated the document for Libero® SoC PolarFire v2.3 release.
- Added information about burst mode receiver, see CDR Options.
- Added information about the alignment of transmit lanes, see Transmit Lane Alignment.
- Added information about Tx loss insertion, see Tx Insertion Loss.
- Added a footnote under Table 34 that describes how to disable the ODT value for the differential REFCLK.
- Added a footnote under Table 32 that describes the minimum pulse width for the PMA reset signal.
|
| Revision 3.0 | 1/18 | The following is a summary of the changes in this revision.- Information about 8b10b, 64b66b, and PMA only features was added. See 8b10b, 64b66b/64b67b, and PMA Only.
- Information about signal integrity was added. See Signal Integrity Conditioning.
- Information about Bit-slip was updated. See Bit Slip. 8b10b does not support bit slip mechanism.
|
| Revision 2.0 | 6/17 | The following is a summary of the changes in this revision.- Information about 8b10b, 64b66b, and PMA only features was added. See 8b10b, 64b66b/64b67b, and PMA Only.
- Information about Word Alignment was added as sub-section to 8b10b. See Word Alignment (Byte Boundary or Comma Detect).
- Updated Figure 52 and Figure 53.
- Information about LANE#_RX_VAL port name description was updated. See Table 4, Table 7, and Table 11.
|
| Revision 1.0 | 2/17 | The first publication of UG0677: PolarFire FPGA Transceiver User Guide. |