Open a serial console
application (Tera Term) with the associated COM port of the RNBD350 module with the
following settings.
Figure 2-17. Testing the Text
Mode
Mobile Side
Follow the same steps
mentioned in Transparent UART Connection section steps 3 to 10 to
establish the Bluetooth Low Energy UART connection with the RNBD350 module.
Tap Text mode to initiate
the data transfer. Figure 2-18. Initiating the Data
Transfer
Enter the text to be transferred
from mobile to the RNBD350 module, then
tap SEND. For example, Hello World!. The RNBD350 module side receives the data,
which is displayed on the serial terminal of the RNBD350 module. Figure 2-19. Serial Terminal of RNBD350
Type any data on the serial
terminal of the RNBD350 module to send
it to the Microchip Bluetooth Data application, which is received and printed on
the receive view of the Microchip Bluetooth Data application. Figure 2-20. Output