2.7.1 Introduction
The RNBD350 module supports a special feature called virtual sniffer. The Bluetooth virtual sniffer allows the user to capture and view live HCI traces in a supported packet analyzer tool (Frontline Wireless protocol suite) that runs locally on their test machine. The virtual sniffing function simplifies Bluetooth development and is easy-to-use functionality. This feature showcases the debug capability of the RNBD350 module, which helps the users to quickly fix issues by capturing and analyzing the packets exchanged between the RNBD350 module and peer device. This feature makes the RNBD350 module a more reliable device for the developers as it can even perform as a wireless packet sniffer, which eliminates the need for extra sniffing hardware.
In addition to the UART used for the data exchange (ASCII command support), the RNBD350 module supports a debug UART (RXD/TXD) to implement the Bluetooth virtual sniffing feature. The log from the device is collected from this debug UART interface, and is, then, fed to the packet analyzer tool. The debug UART operates in 921600 baud rate, and it is not configurable.