4.3.3.2 Obtaining a Disk ID

Paid licenses are available as node-locked and floating licenses. When installing a node-locked license, you are prompted for a disk ID.

A node-locked license is locked to a specific hard disk ID. This ID, also referred to as a disk ID, is the hard drive serial number of the computer on which the license will be installed. A disk ID is an 8-character hexadecimal number of the form xxxx-xxxx (for example, A085-AFE9).

When specifying the disk ID, use the disk ID of the system drive (the C:\ drive), even if you install the Libero SoC Design Suite on another drive. Remote Desktop is not supported.

To obtain your computer's disk ID, type the following command at the command prompt: C:> Vol C:

When the disk ID is returned, enter it where indicated on the registration page.