Description
This Tcl
command processes a job request received from Job Manager. It is part of the Job
Ticket generation process.
Important: HSM server name must be specified via HSM_SERVER_NAME DEF
variable.
process_job_request -request_file "job request file" \
-reply_file "job reply file" \
[-overwrite_reply "TRUE | FALSE"]
Arguments
Parameter | Type | Description |
---|
request_file | string | Specifies full file name of job request file. This parameter is
mandatory. |
reply_file | string | Specifies full file name of job reply file. This parameter is
mandatory. |
overwrite_reply | boolean | This parameter is optional. The possible value of this parameter
are the following: - TRUE or 1:
Allows overwriting of any pre-existing reply_file.
- FALSE or 0:
Does not allow overwriting of any pre-existing
reply_file.
|
Return Type | Description |
---|
None | None |
Error Codes
Error Code | Description |
---|
None | Required parameter 'request_file' is missing. |
None | Required parameter 'reply_file' is missing. |
None | Parameter 'request_file' : the file '/request_file_name' does not
exist. |
None | overwrite_reply: Invalid argument value: 'value' (expecting TRUE,
1, true, FALSE, 0 or false). |
None | Cannot get HSM. |
None | Parameter 'param_name' is not defined. Valid command formatting
is 'process_job_request -request_file "job request file" \
-reply_file "job reply file" \ [-overwrite_reply "TRUE |
FALSE"]'. |
Supported Families
PolarFire® |
SmartFusion® 2 |
IGLOO® 2 |
PolarFire SoC |
Example
This example
processes a job
request:
process_job_request \
-request_file {D:/flashpro_files/jobmgr_project/cm_request.req} \
-reply_file {D:/flashpro_files/jobmgr_project/cm_reply.rep} \
-overwrite_reply {TRUE}
See Also
- set_hsm_params
- create_job_project