1.2.8 Hot-Join Does Not Work Properly When RETRY
= 1
If a Hot-Join request is NACK'd when the retry limit is 1 (I3CxRETRY =
1), the module may not exit the Hot-Join state and continue making more
Hot-Join requests until the request is ACK'd by the controller. This behavior is similar
to an unlimited retry limit (I3CxRETRY = 0).
Work around
The user should set a retry limit value greater than 1 (I3CxRETRY >
1).
Affected Silicon Revisions
| B2 |
| X |