closesocket Function
C
int closesocket(
SOCKET s
);
Description
The closesocket function closes an existing socket. This function releases the socket descriptor s. Any data buffered at the socket is discarded. If the socket s is no longer needed, closesocket() must be called in order to release all resources associated with s.
Preconditions
None.
Parameters
Parameters | Description |
---|---|
s | Socket descriptor returned from a previous call to socket. |
Returns
- 0 - The function was successful.
- SOCKET_ERROR (-1) - Function failed. errno is set accordingly.
Remarks
None.