accept Function
C
SOCKET accept(
SOCKET s,
struct sockaddr* addr,
int* addrlen
);
Description
The accept function is used to accept connection request queued for a listening socket. If a connection request is pending, accept removes the request from the queue, and a new socket is created for the connection. The original listening socket remains open and continues to queue new connection requests. The socket must be a SOCK_STREAM type socket.
Preconditions
The listen function should be called.
Parameters
Parameters | Description |
---|---|
s | Socket descriptor returned from a previous call to socket. Must be bound to a local name and in listening mode. |
addr | Optional pointer to a buffer that reveives the address of the connecting entity. |
addrlen | Optional pointer to an integer that contains the length of the address addr. |
Returns
- non-negative integer - The function succeeds and the integer is a descriptor for the accepted socket.
- SOCKET_ERROR - Function failed. errno is set accordingly.
Remarks
None.