bind Function
C
int bind(
SOCKET s,
const struct sockaddr* name,
int namelen
);
Description
The bind function assigns a name to an unnamed socket. The name represents the local address of the communication endpoint. For sockets of type SOCK_STREAM, the name of the remot endpoint is assigned when a connect or accept function is executed.
Preconditions
The socket function should be called.
Parameters
Parameters | Description |
---|---|
s | Socket descriptor returned from a previous call to socket. |
name | Pointer to the sockaddr structure containing the local address of the socket. |
namelen | Length of the sockaddr structure. |
Returns
- 0 - The function was successful.
- SOCKET_ERROR - Function failed. errno is set accordingly.
Remarks
None.