TCPIP_FTP_MODULE_CONFIG Structure
C
typedef struct {
uint16_t cmdPort;
uint16_t dataPort;
uint16_t nConnections;
uint16_t dataSktTxBuffSize;
uint16_t dataSktRxBuffSize;
const char* mountPath;
char * userName;
char * password;
} TCPIP_FTP_MODULE_CONFIG;
Description
Structure: TCPIP_FTP_MODULE_CONFIG.
FTP server configuration and initialization data. Configuration is part of tcpip_stack_init.c.
Members
| Members | Description |
|---|---|
| cmdPort | FTP listening command port: TCPIP_FTP_COMMAND_PORT (21, 990, etc.). |
| dataPort | FTP listening data port: TCPIP_FTP_DATA_PORT (20, 989) etc. |
| nConnections | Number of simultaneous FTP connections allowed. |
| dataSkTxBuffSize | Size of data socket TX buffer for the associated socket. Leave 0 for default. |
| dataSktRxBuffSize | Size of data socket RX buffer for the associated socket. Leave 0 for default. The FTP server will access files located under this top directory. No access is possible above this directory. As a good practive to follow, use something like: "/mnt_point/ftp/" to limit an external user access to this only directory in the file system when accessing files. |
| userName | FTP login user name. Size should not exceed more than TCPIP_FTP_USER_NAME_LEN. |
| password | FTP login password. Size should not exceed more than TCPIP_FTP_PASSWD_LEN. |
Remarks
The obsolete authentication members will be eventually removed from the FTP server module configuration data. New projects should use the run time authentication.