| Macros | |
| ARP_CACHE_DELETE_OLD | On initialization, delete the old cache if still in place Else don't re-initialize Default should be 1 |
| TCPIP_ARP_CACHE_ENTRIES | Number of entries in the cache. Default number of entries per interface. |
| TCPIP_ARP_CACHE_ENTRY_RETRIES | Number of ARP requests generated for resolving an entry. |
| TCPIP_ARP_CACHE_PENDING_ENTRY_TMO | Timeout for a cache entry pending to be solved, in seconds. The entry will be removed if the tmo elapsed and the entry has not been solved. A solved entry moves to the solved entries timeout. |
| TCPIP_ARP_CACHE_PENDING_RETRY_TMO | Timeout for resending an ARP request for a pending entry. In order to prevent the ARP flooding the standard recommends it to be greater than 1 sec. It should be less than TCPIP_ARP_CACHE_PENDING_ENTRY_TMO |
| TCPIP_ARP_CACHE_PERMANENT_QUOTA | Max percentage of permanent entries in the cache. Note that since permanent entries cannot be removed they tend to degrade the efficiency of the cache look up. |
| TCPIP_ARP_CACHE_PURGE_QUANTA | The number of entries to delete, once the threshold is reached. |
| TCPIP_ARP_CACHE_PURGE_THRESHOLD | Default purge threshold, percentage Once the number of resolved entries in the cache gets beyond the threshold some resolved entries will be purged. |
| TCPIP_ARP_CACHE_SOLVED_ENTRY_TMO | Timeout for a solved entry in the cache, in seconds. The entry will be removed if the tmo elapsed and the entry has not been referenced again |
| TCPIP_ARP_GRATUITOUS_PROBE_COUNT | Number of ARP requests generated when sending a gratuitous ARP probe. Default value should be 1. |
| TCPIP_ARP_TASK_PROCESS_RATE | ARP task processing rate, in milliseconds. The ARP module will process a timer event with this rate for maintaining its own queues, processing timeouts, etc. Choose it so that the other ARP_CACHE_xxx_TMO are multiple of this The default value is 2 seconds. The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained The value cannot be lower than the TCPIP_STACK_TICK_RATE. |
| TCPIP_ARP_PRIMARY_CACHE_ONLY | ARP caches configuration for aliases. If this symbol is true, then the alias interfaces share the cache with the primary interface. Otherwise each interface uses its own cache. Default value should be 1 if the alias interfaces are in the same network with the primary interface |
| General Functions | |
| TCPIP_ARP_HandlerDeRegister | Deregisters the event handler |
| TCPIP_ARP_HandlerRegister | Register an ARP resolve handler. |
| TCPIP_ARP_EntryGet | Gets the current mapping for an IP address. |
| TCPIP_ARP_EntryRemove | Removes the mapping of an address, even a permanent one |
| TCPIP_ARP_EntryRemoveNet | Removes all the entries belonging to a network interface. |
| TCPIP_ARP_EntrySet | Adds an ARP cache entry for the specified interface. |
| TCPIP_ARP_IsResolved | Determines if an ARP request has been resolved yet. |
| TCPIP_ARP_Probe | Transmits an ARP probe to resolve an IP address. |
| TCPIP_ARP_Resolve | Transmits an ARP request to resolve an IP address. |
| TCPIP_ARP_Task | Standard TCP/IP stack module task function. |
| Cache Manipulation Functions | |
| TCPIP_ARP_CacheEntriesNoGet | Used to retrieve the number of entries for a specific interface. |
| TCPIP_ARP_CacheThresholdSet | Sets the cache threshold for the specified interface in percent. |
| TCPIP_ARP_EntryQuery | Queries an ARP cache entry using the index of the cache line. |
| TCPIP_ARP_EntryRemoveAll | Removes all the mapping belonging to an interface. |
| Data Types and Constants | |
| TCPIP_ARP_ENTRY_QUERY | ARP entry query. |
| TCPIP_ARP_ENTRY_TYPE | Type of ARP entry. |
| TCPIP_ARP_EVENT_HANDLER | Notification handler that can be called when a specific entry is resolved. |
| TCPIP_ARP_EVENT_TYPE | Events reported by ARP. |
| TCPIP_ARP_HANDLE | ARP handle. |
| TCPIP_ARP_OPERATION_TYPE | Type of ARP operation. |
| TCPIP_ARP_RESULT | ARP results (success and failure codes). |
| TCPIP_ARP_MODULE_CONFIG | This is type TCPIP_ARP_MODULE_CONFIG. |