TCPIP_ARP_Resolve Function
C
TCPIP_ARP_RESULT TCPIP_ARP_Resolve(
TCPIP_NET_HANDLE hNet,
IPV4_ADDR* IPAddr
);
Description
This function transmits and ARP request to determine the hardware address of a given IP address. Upon the address resolution it calls the registered handler (if available) with the supplied notification parameter (if != 0).
Preconditions
The ARP module should have been initialized.
Parameters
| Parameters | Description |
|---|---|
| hNet | Interface to use. |
| IPAddr | The IP address to be resolved. The address must be specified in network byte order (big endian). |
Returns
An element from the TCPIP_ARP_RESULT enumeration.
ARP_RES_ENTRY_SOLVED - if the required entry is already solved.
ARP_RES_ENTRY_QUEUED - if the required entry was already queued.
ARP_RES_ENTRY_NEW - if the operation succeeded and a new entry was added (and queued for resolving).
ARP_RES_CACHE_FULL - if new entry could not be inserted, the cache was full.
ARP_RES_BAD_ADDRESS - bad address specified.
ARP_RES_NO_INTERFACE - no such interface.
Remarks
To retrieve the ARP query result, call the TCPIP_ARP_IsResolved function.