DRV_GMAC_Open Function
C
DRV_HANDLE DRV_GMAC_Open(const SYS_MODULE_INDEX drvIndex, const DRV_IO_INTENT intent); Returns
DRV_HANDLE - handle (pointer) to MAC client
0 if call failed
Description
This function opens a client instance of the PIC32 MAC Driver. Used by tcpip_module_manager.
Remarks
The intent parameter is not used in the current implementation and is maintained only for compatibility with the generic driver Open function signature.
Preconditions
DRV_GMAC_Initialize() should have been called.