DRV_GMAC_PowerMode Function
C
bool DRV_GMAC_PowerMode(DRV_HANDLE hMac, TCPIP_MAC_POWER_MODE pwrMode); Returns
true if the call succeeded.
false if the call failed
Description
This function sets the power mode for the Ethernet MAC.
Remarks
This function is not currently supported by the Ethernet MAC and will always return true.
Preconditions
DRV_GMAC_Initialize must have been called to set up the driver. DRV_GMAC_Open() should have been called to obtain a valid handle.